DOCA0272EN-00

System Asset Management

Function block profile

Function block type

System avatar function block

Type of data access

Acyclic (read)

Intended use

System avatar (Bus coupler)

Functionality

The System Asset Management function block returns the status of the acyclic asset management data of the System avatar.

The following sections provide detailed information about the interface and the use of the parameters of the PROFINET IO and PROFIBUS DP function blocks for this avatar.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.