DOCA0272EN-00

PN_SystemTime (PROFINET IO)

The following tables give information about the parameters of the function block interface.

Inputs

Input

Data Type

Description

Variable Category

i_xEnable

BOOL

Activates the function block processing. Cyclic data will be read/written to the hardware IO interface.

Function block control

i_xAcyclicBusy

BOOL

Can be used to block the acyclic execution if acyclic communication of another function block is active.

Function block control

i_xGetSysTime

BOOL

If this input is set to TRUE, the system time of the Bus coupler is read to the engineering system.

Function block control

i_xSetSysTime

BOOL

If this input is set to TRUE, the engineering system time is written to the Bus coupler.

Function block control

i_dtlSysTime

DTL

Corresponds to engineering system time written to the Bus coupler.

Acyclic data

i_hwSubmHWID

HW_IO

Must correspond to the hardware identifier of the acyclic submodule of the related avatar to be able to execute the acyclic communication.

Communication parameter

Outputs

Output

Data Type

Description

Variable Category

q_xActive

BOOL

If this output is set to TRUE, the Avatar function block is enabled, or an acyclic request is busy.

Function block status

q_xError

BOOL

If this output is set to TRUE, a detected error occurred while executing the Avatar function block. For detailed information about the detected error, see the value of the Error ID.

Function block status

q_dwErrorID

DWORD

The Error ID shows detailed information about the detected error that occurred. Possible values are shown in the table below.

Function block status

q_dwAcyclicStatus

DWORD

The Acyclic status provides detailed information about the acyclic fieldbus communication, including detected error details. For detailed information about the status values, see Function Block Library.

Function block status

q_xAcyclicBusy

BOOL

If this output is set to TRUE, an acyclic request is still busy.

Function block status

q_dtlSysTime

DTL

Corresponds to the system time read from the Bus coupler.

Acyclic data

Status and error codes from ConstTeSysIsland

Member name

Used by the function block

Cdw_ErrNoMsg

Yes

Cdw_ErrInternal

Yes

Cdw_ErrInvalidCycInAddr

No

Cdw_ErrInvalidHwid

Yes

Cdw_ErrInvalidNumOfAvatars

No

Cdw_ErrReadCycIn

No

Cdw_ErrReadAcycData1

Yes

Cdw_ErrReadAcycData2

No

Cdw_ErrWriteAcycData

Yes

Cdw_StsReadAcycData1Compl

Yes

Cdw_StsReadAcycData2Compl

No

Cdw_StsWriteAcycDataCompl

Yes

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.