DOCA0272EN-00

UDT_Control

The Control UDT is used to transfer the acyclic control data of an avatar, like alarm and trip messages. The interfaces of all PROFINET IO and PROFIBUS DP Control avatar function blocks contain this UDT as a parameter.

Not all Alarm and Trip Message bits are supported by all Control avatars. Details of which bits are supported by the individual avatars are included in the descriptions of the Avatar Control Function Blocks.

Elements

Element

Data Type

Description

MotorTemperature

UINT

Indicates the temperature of the motor in increments of 0.1 °C. Depending on the temperature sensor type, the range is as follows:

  • –200 to 850 °C (–328 to 1562 °F) (for PT100)

  • –200 to 600 °C (–328 to 1112 °F) (for PT1000)

  • –60 to 180 °C (–76 to 356 °F) (for NI 100/1000)

SIL* Group

USINT

Indicates the number of the SIL group.

ThermalCapacity

USINT

Provides the percentage (%) of the thermal capacity of the motor.

AlarmMsg1

STRUCT

The alarm messages of a Control avatar. See Struct AlarmMsg1.

AlarmMsg2

STRUCT

The alarm messages of a Control avatar. See Struct AlarmMsg2.

TripMsg1

STRUCT

The trip messages of a Control avatar. See Struct TripMsg1.

TripMsg2

STRUCT

The trip messages of a Control avatar. See Struct TripMsg2.

TimeToTrip

UINT

Estimated time (s) before a Thermal Overload trip will occur given the current conditions.

TimeToReset

UINT

Estimated time to wait before a reset could acknowledge a Thermal Overload trip.

PAStatusReg1

Struct

Predictive Alarm Status Register 1

Struct AlarmMsg1

Element

Data Type

BIT

Description

(reserved)

BOOL

8

 

(reserved)

BOOL

9

 

(reserved)

BOOL

10

 

(reserved)

BOOL

11

 

(reserved)

BOOL

12

 

(reserved)

BOOL

13

 

(reserved)

BOOL

14

 

(reserved)

BOOL

15

 

(reserved)

BOOL

0

 

(reserved)

BOOL

1

 

GroundCurrent

BOOL

2

The avatar has detected the conditions to cause a ground current event.

ThermalOverload

BOOL

3

The avatar thermal capacity has increased above the thermal overload level.

(reserved)

BOOL

4

 

Jam

BOOL

5

The avatar has detected the conditions to cause a jam event.

CurrentPhaseUnbalance

BOOL

6

The avatar has detected the conditions to cause a current phase unbalance event.

UnderCurrent

BOOL

7

The avatar has detected the conditions to cause an undercurrent event.

Struct AlarmMsg2

Element

Data Type

BIT

Description

(reserved)

BOOL

8

 

(reserved)

BOOL

9

 

(reserved)

BOOL

10

 

(reserved)

BOOL

11

 

(reserved)

BOOL

12

 

(reserved)

BOOL

13

 

(reserved)

BOOL

14

 

(reserved)

BOOL

15

 

(reserved)

BOOL

0

 

(reserved)

BOOL

1

 

(reserved)

BOOL

2

 

OverCurrent

BOOL

3

The avatar has detected the conditions to cause an overcurrent event.

(reserved)

BOOL

4

 

(reserved)

BOOL

5

 

MotorOverheat

BOOL

6

The motor temperature has increased above the motor overheat level.

(reserved)

BOOL

7

 

Struct TripMsg1

Element

Data Type

BIT

Description

Stall

BOOL

8

The avatar has detected the conditions to cause a stall trip event.

(reserved)

BOOL

9

 

(reserved)

BOOL

10

 

(reserved)

BOOL

11

 

(reserved)

BOOL

12

 

(reserved)

BOOL

13

 

(reserved)

BOOL

14

 

(reserved)

BOOL

15

 

(reserved)

BOOL

0

 

(reserved)

BOOL

1

 

GroundCurrent

BOOL

2

The avatar has detected the conditions to cause a ground current trip event.

ThermalOverload

BOOL

3

The avatar thermal capacity has increased above 100%.

LongStart

BOOL

4

The avatar has detected the conditions to cause a long start trip event.

Jam

BOOL

5

The avatar has detected the conditions to cause a jam trip event.

CurrentPhaseUnbalance

BOOL

6

The avatar has detected the conditions to cause a current phase unbalance trip event.

UnderCurrent

BOOL

7

The avatar has detected the conditions to cause an undercurrent trip event.

Struct TripMsg2

Element

Data Type

BIT

Description

(reserved)

BOOL

8

 

(reserved)

BOOL

9

 

(reserved)

BOOL

10

 

(reserved)

BOOL

11

 

(reserved)

BOOL

12

 

(reserved)

BOOL

13

 

(reserved)

BOOL

14

 

(reserved)

BOOL

15

 

(reserved)

BOOL

0

 

(reserved)

BOOL

1

 

PhaseConfig

BOOL

2

The avatar has detected the conditions to cause a phase configuration trip event.

OverCurrent

BOOL

3

The avatar has detected the conditions to cause an overcurrent trip event.

CurrentPhaseLoss

BOOL

4

The avatar has detected the conditions to cause a current phase loss trip event.

CurrentPhaseReversal

BOOL

5

The avatar has detected the conditions to cause a current phase reversal trip event.

MotorOverheat

BOOL

6

The motor temperature has increased above the motor overheat trip level.

(reserved)

BOOL

7

 

Struct PAStatusReg1

Element

Data Type

BIT

Description

PA8Status

BOOL

8

Status of Predictive Alarm Bit 8

PA9Status

BOOL

9

Status of Predictive Alarm Bit 9

(reserved)

BOOL

10

 

(reserved)

BOOL

11

 

(reserved)

BOOL

12

 

(reserved)

BOOL

13

 

(reserved)

BOOL

14

 

(reserved)

BOOL

15

 

PA0Status

BOOL

0

Status of Predictive Alarm Bit 0

PA1Status

BOOL

1

Status of Predictive Alarm Bit 1

PA2Status

BOOL

2

Status of Predictive Alarm Bit 2

PA3Status

BOOL

3

Status of Predictive Alarm Bit 3

PA4Status

BOOL

4

Status of Predictive Alarm Bit 4

PA5Status

BOOL

5

Status of Predictive Alarm Bit 5

PA6Status

BOOL

6

Status of Predictive Alarm Bit 6

PA7Status

BOOL

7

Status of Predictive Alarm Bit 7

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.