DOCA0272EN-00

Device Asset Management Function Blocks

All Device Asset Management function blocks share the same set of detected error codes as stated in the following table:

Status and error codes from ConstTeSysIsland

Member name

Used by the function block

Cdw_ErrNoMsg

Yes

Cdw_ErrInternal

Yes

Cdw_ErrInvalidCycInAddr

No

Cdw_ErrInvalidHwid

Yes

Cdw_ErrInvalidNumOfAvatars

No

Cdw_ErrReadCycIn

No

Cdw_ErrReadAcycData1

Yes

Cdw_ErrReadAcycData2

No

Cdw_ErrWriteAcycData

No

Cdw_StsReadAcycData1Compl

Yes

Cdw_StsReadAcycData2Compl

No

Cdw_StsWriteAcycDataCompl

No

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.