DOCA0272EN-00

Function Blocks

The following sections define the interfaces of each of the function blocks of the library, their functionality, and their intended use. Besides names, data types, and a description, for each interface variable of the function blocks, one of the following categories is specified:

Categories

Category

Meaning

Function block control

Input variable to control the execution of the function block (for example, trigger acyclic communication).

Function block status

Output variable that gives information on the status of the function block execution.

Communication parameter

Input or in/out variable used to parametrize either cyclic or acyclic data access.

Cyclic data

Input or output variable that is part of the data transferred through cyclic communication to or from TeSys™ island.

Acyclic data

Input or output variable that is part of the data transferred through acyclic communication to or from TeSys™ island.

Additionally, the sections document which values (e.g. which common error and status codes) from ConsTeSysisland (see Data Block ConstTeSysIsland) are used by each of the function blocks.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.