AO Settings
Description
The TeSys Tera system supports up to two analog outputs (AO) with two LTMTAN21 expansion modules.
Parameter Setting
Each AO Settings function has the following configurable settings:
|
Parameter |
Setting range |
Default value |
|---|---|---|
|
AO1 Source |
|
None |
Analog Output Source Settings
The table lists the minimum and maximum setting values for each analog output source.
|
Analog Output source |
Default Value |
AO1 source minimum range |
AO1 source maximum range |
|---|---|---|---|
|
None |
None |
0 |
0 |
|
L1 RMS current |
10 %FLC1 |
10 %FLC1 |
1000 %FLC1 |
|
L2 RMS current |
10 %FLC1 |
10 %FLC1 |
1000 %FLC1 |
|
L3 RMS current |
10 %FLC1 |
10 %FLC1 |
1000 %FLC1 |
|
Average current |
10 %FLC1 |
10 %FLC1 |
1000 %FLC1 |
|
L1-L2 RMS voltage |
20 %Vn |
20 %Vn |
150 %Vn |
|
L2-L3 RMS voltage |
20 %Vn |
20 %Vn |
150 %Vn |
|
L3-L1 RMS voltage |
20 %Vn |
20 %Vn |
150 %Vn |
|
Average voltage |
20 %Vn |
20 %Vn |
150 %Vn |
|
System frequency |
50 %NominalHz |
50 %NominalHz |
150 %NominalHz |
|
Total active power |
20 %Pn |
20 %Pn |
1000 %Pn |
|
Total apparent power |
20 %Pn |
20 %Pn |
1000 %Pn |