DOCA0257EN-01

Stall Rotor

Description

The Stall Rotor condition occurs when the motor is in the Run state and occurs due to overload or the load jam. The Stall Rotor protection function is active only when the motor is in the Run state.

The Stall Rotor protection function generates the following signals:

  • Alarm: Any of the three-phase currents of the motor goes above the alarm level during the motor Run state.

  • Trip: Any of the three-phase currents of the motor goes above the pickup level for the specified time delay during the motor Run state.

Parameter Setting

The Stall Rotor protection function has the following configurable settings:

Parameter

Setting range

Default value

Function

  • Disable

  • Alarm
  • Trip
  • Alarm + Trip

Trip

Pickup

50–1000% of IFLC in step of 1%

200% of IFLC

Time Delay

0.1–6000.0 s in step of 0.1 s

2 s

Alarm Level

50–1000% of IFLC in step of 1%

200% of IFLC

Reset Mode

  • Reset key

  • DI

  • Communication

  • Auto

DI + Reset Key

Auto-Reset Delay (applicable only if Reset mode is Auto)

0.0–6000.0 s in step of 0.1 s

0 s

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.