DOCA0257EN-01

Current Phase Sequence

The LTMT main unit detects the current phase sequence of three-phase motor supply.

  • L123: L1 current at angle 0°, L2 current at angle 240°, L3 current at angle 120°.

  • L132: L1 current at angle 0°, L2 current at angle 120°, L3 current at angle 240°.

  • CTWF: Current transformer wiring trip detected by the LTMT main unit. For example, one of the three phases is wired in opposite direction.

NOTE: Current phase sequence is not available in single-phase mode.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?