DOCA0257EN-01

Temperature Protection

Description

The TeSys Tera system supports temperature inputs:

  • One temperature input on LTMT main unit, that can be configured as PT100 or PTC.

The temperature protection function generates the following signals:

  • Alarm: Temperature value goes above the alarm level.

  • Trip: Temperature value goes above the trip level for the desired time delay.

LTMT Main Unit Parameter Setting

The temperature protection function of the LTMT main unit has the following configurable settings:

Parameter

Setting range

Default value

Function

  • Disable

  • Alarm
  • Trip
  • Alarm + Trip

Disable

PT100 trip level (applicable if PT100 sensor is selected)

25.0–180.0 °C in step of 0.1 °C

130.0 °C

PTC trip level (applicable if PTC sensor is selected)

2700–4000 Ω in step of 1 Ω

2700 Ω

PTC trip level reset (if PTC sensor is selected)

1600–2300 Ω in step of 1 Ω

1600 Ω

Time Delay

0.1–6000.0 s in step of 0.1 s

1 s

PT100 alarm level (applicable if PT100 sensor is selected)

25.0–180.0 °C in step of 0.1 °C

130.0 °C

Reset Mode

  • Reset key

  • DI

  • Communication

  • Auto

DI + Reset Key

Auto-Reset Delay (applicable only if Reset mode is Auto)

0.0–6000.0 s in step of 0.1 s

0 s

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?