DOCA0257EN-01

Analog Input Protection

Description

There are maximum four analog inputs possible with maximum of two LTMTAN21 expansion modules. For each LTMT expansion module, the analog input (AI) are provided with protection function.

The AI Protection function generates the following signals:

  • Alarm:

    • For detection setting Under, if the analog input goes below the alarm level

    • For detection setting Over, if the analog input goes above the alarm level

  • Trip:

    • For detection setting Under, if the analog input goes below the trip level for the desired time delay

    • For detection setting Over, if the analog input goes above the trip level for the desired time delay

Parameter Setting

Each AI Protection function has the following configurable settings:

Parameter

Setting range

Default value

Function

  • Disable

  • Alarm
  • Trip
  • Alarm + Trip

Disable

Detection

  • Under

  • Over

Under

Trip level

4.0–20.0 mA in step of 0.1 mA

4.0 mA

Time delay

0.0–6000.0 s in step of 0.1 s

0.0 s

Alarm

4.0–20.0 mA in step of 0.1 mA

4.0 mA

Reset mode

  • Auto

  • DI

  • Communication

  • Reset Key

DI + Reset Key

Auto Reset Delay (applicable only if Reset mode is Auto)

0.0–6000.0 s in step of 0.1 s

0.0 s

Diagnostic

  • Disable

  • Enable

Disable

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.