DOCA0257EN-01

Over Power

Description

The Over Power protection function generates the following signals:

  • Alarm: Measured active power goes above the alarm level.

  • Trip: Measured active power goes above the trip level for the specified time delay.

Parameter Setting

The Over Power protection function has the following configurable settings:

Parameter

Setting range

Default value

Function

  • Disable

  • Alarm
  • Trip
  • Alarm + Trip

Disable

Trip Level

20–1000% of nominal power in step of 1%

110% of nominal power

Time Delay

0.1–6000.0 s in step of 0.1 s

0.1 s

Alarm Level

20–1000% of nominal power in step of 1%

110% of nominal power

Reset Mode

  • Reset key

  • DI

  • Communication

  • Auto

DI + Reset Key

Auto-Reset Delay (applicable only if Reset mode is Auto)

0.0–6000.0 s in step of 0.1 s

0 s

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.