DOCA0257EN-01

Thermal Time to Cool

Description

The LTMT main unit displays the time to cool when motor is stopped or tripped. Based on the trip class and service factor parameters of thermal overload protection settings, the LTMT main unit calculates the time to cool and keeps the LTMT main unit in inhibit state.

Characteristics

Characteristic

Value

Unit

s

Resolution

1 s

Refresh interval

1 s

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?