DOCA0257EN-01

Analog Output Measurement

A maximum of two analog outputs can be connected to two LTMTAN21 expansion modules to get analog measurements. Each module has one analog outputs.

Characteristic

Value

Range

4–20 mA

Unit

mA

Resolution

0.1

Refresh Interval

100 ms

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.