DOCA0257EN-01

About the Document

Document Scope

This guide provides complete information necessary to use the TeSys Tera system which includes:

  • LTMT main unit

  • LTMTCT/LTMTCTV sensor modules

  • LTMT expansion module
  • LTMTCUF control operator unit

The purpose of this guide is to:

  • Provide information necessary to configure and operate the TeSys Tera system and its components

  • Describe the metering, monitoring, protection, and control functions of the TeSys Tera system

This guide is intended for:

  • Design engineers

  • System integrators

  • System operators

Validity Note

This document is valid for the following certified components of the TeSys Tera system:

Commercial Reference

Description

Range

LTMTEFM

LTMT main unit with EtherNet/IP or Modbus TCP/IP protocol

100–240 Vac/Vdc

LTMTEBD

LTMT main unit with EtherNet/IP or Modbus TCP/IP protocol

24 Vdc

LTMTMFM

LTMT main unit with Modbus RTU protocol

100–240 Vac/Vdc

LTMTMBD

LTMT main unit with Modbus RTU protocol

24 Vdc

LTMTPFM

LTMT main unit with PROFIBUS DP protocol

100–240 Vac/Vdc

LTMTPBD

LTMT main unit with PROFIBUS DP protocol

24 Vdc

LTMTCT3T

LTMT horizontal sensor module with current transformer

Current range = 0.3–3 A

LTMTCT25T

LTMT horizontal sensor module with current transformer

Current range = 2.5–25 A

LTMTCT100T

LTMT horizontal sensor module with current transformer

Current range = 10–100 A

LTMTCTV3T

LTMT horizontal sensor module with current and voltage transformers

  • Current range = 0.3–3 A

  • Voltage range = 60–690 Vac

LTMTCTV25T

LTMT horizontal sensor module with current and voltage transformers

  • Current range = 2.5–25 A

  • Voltage range = 60–690 Vac

LTMTCTV100T

LTMT horizontal sensor module with current and voltage transformers

  • Current range = 10–100 A

  • Voltage range = 60–690 Vac

LTMTCTV3UT

LTMT horizontal sensor module with current and voltage transformers

  • Current range = 0.3–3 A

  • Voltage range = 60–600 Vac

LTMTCTV25UT

LTMT horizontal sensor module with current and voltage transformers

  • Current range = 2.5–25 A

  • Voltage range = 60–600 Vac

LTMTCTV100UT

LTMT horizontal sensor module with current and voltage transformers

  • Current range = 10–100 A

  • Voltage range = 60–600 Vac

LTMTIN42FM

LTMT expansion module with four digital inputs and two digital outputs

  • 100–265 Vac/dc for IEC

  • 110–240 Vac/dc for UL

LTMTIN42BD

LTMT expansion module with four digital inputs and two digital outputs

24 Vdc

LTMTAN21

LTMT expansion module with two analog inputs and one analog output

4–20 mA

LTMT9RJ1015

LTMT main unit to LTMTCT/LTMTCTV sensor module RJ11 connector cable

0.15 m (5.9 in) in length

LTMT9RJ105

LTMT main unit to LTMTCT/LTMTCTV sensor module RJ11 connector cable

0.5 m (19.6 in) in length

LTMTCUF

LTMTCUF control operator unit

LTMT9RJ102

LTMT main unit to LTMTCT/LTMTCTV sensor module cable

0.2 m (7.874 in) in length

LTMT9RJ401

LTMT main unit to LTMT expansion module RJ45 connector cable

0.1 m (3.9 in) in length

LTMT9EX10

LTMT main unit to LTMT expansion module cable

1 m (39.37 in) in length

LTMT9CU10S

LTMT main unit to LTMTCUF control operator unit

1 m (39.37 in) in length

LTMT9CU30S

LTMT main unit to LTMTCUF control operator unit

3 m (118.11 in) in length

The availability of some functions described in this document depends on the communication protocol used and the physical modules installed on the TeSys Tera system.

General Cybersecurity Information

In recent years, the growing number of networked machines and production plants has seen a corresponding increase in the potential for cyber threats, such as unauthorized access, data breaches, and operational disruptions. You must, therefore, consider all possible cybersecurity measures to help protect assets and systems against such threats.

To help keep your Schneider Electric products secure and protected, it is in your best interest to implement the cybersecurity best practices as described in the Cybersecurity Best Practices document.

Schneider Electric provides additional information and assistance:

Product Related Cybersecurity Information

Environmental Data

For product compliance and environmental information, refer to the Schneider Electric Environmental Data Program.

Available Languages of the Document

The document is available in these languages:

  • English

  • Chinese

  • French

  • German

  • Italian

  • Korean

  • Spanish

Related Documents

Title of documentation

Description

Reference number

TeSys Tera Motor Management System Catalog

The catalog

  • Describes the TeSys Tera system

  • Contains the TeSys Tera technical characteristics

LVCATENTER

TeSys Tera Motor Management System Installation Guide

This guide describes the installation, commissioning, and maintenance of the LTMT main unit, LTMTCT/LTMTCTV sensor modules, LTMT expansion module, and LTMTCUF control operator unit.

DOCA0356EN

TeSys Tera Motor Management System Modbus RTU Communication Guide

This guide describes the Modbus RTU network protocol communication of the LTMT main unit.

DOCA0355EN

TeSys Tera Motor Management System PROFIBUS DP Communication Guide

This guide describes the PROFIBUS DP network protocol communication of the LTMT main unit.

DOCA0256EN

TeSys Tera Motor Management System LTMTCUF User Guide

This guide describes how to install, configure, and use the LTMTCUF control operator unit.

DOCA0233EN

TeSys Tera Motor Management System DTM Library Online Help Guide

This guide describes the TeSys Tera DTM library which allows the customization of the control functions of the TeSys Tera Motor Management System.

DOCA0275EN

TeSys Tera Motor Management System DTM Library Release Note

This document provides important information about the TeSys Tera DTM

DOCA0279EN

TeSys Tera Motor Management System Firmware Release Note

This guide provides important information about the TeSys Tera system firmware packages and provides summary of new features and enhancement.

DOCA0276EN

TeSys Tera Motor Management System EtherNet/IP Communication Guide

This guide describes the EtherNet/IP network protocol communication of the LTMT main unit.

DOCA0258EN

TeSys Tera Motor Management System Cybersecurity Guide

This guide provides information on cybersecurity aspects for the TeSys Tera Motor Management System. This guide addresses on how to secure your operational technology network, or your company serial or Ethernet network.

DOCA0260EN

To find documents online, visit the Schneider Electric download center (www.se.com/ww/en/download/).

Information on Non-Inclusive or Insensitive Terminology

As a responsible, inclusive company, Schneider Electric is constantly updating its communications and products that contain non-inclusive or insensitive terminology. However, despite these efforts, our content may still contain terms that are deemed inappropriate by some customers.

Trademarks

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.