DOCA0257EN-01

Motor History

Maximum Start Counter

The LTMT main unit counts the number of motor starts within a given period of time. The number of motor starts is used by the function Maximum Number of Starts.

Maximum Start Inhibit Time

The LTMT main unit tracks the maximum start inhibit time. The maximum start inhibit time is defined by the function Maximum Number of Starts.

Motor Starting Peak Current

The LTMT main unit tracks the maximum current drawn by the motor during the start time. When the motor goes to Start state, the LTMT main unit starts recording the starting peak current. When the motor goes to Run or Stop state, the LTMT main unit stops recording the starting peak current.

Motor Starting Time

The LTMT main unit records the time when the motor goes to Start state. The LTMT main unit stops recording the time when the motor goes to Run or Stop state.

Total Run Hour

The LTMT main unit records the total run hour from the factory reset or Reset total run hour command.

Last Run Hour

The LTMT main unit measures the number of hours the motor has run from the time it has last been started.

Number of Starts

The LTMT main unit counts the total number of times the motor has started.

The number of starts is reset to zero by:

  • Return to default values command.

  • Reset number of starts command.

Number of Stops

The LTMT main unit counts the total number of times the motor has stopped.

The number of stops is reset to zero by:

  • Return to default values command.

  • Reset number of stops command.

Motor Stop Cause

Motor stop cause

Description

HMI

Motor stopped on command received from LTMTCUF control operator unit.

Local DI

Motor stopped on Local Stop DI input detection.

Remote DI

Motor stopped on Remote DI input detection.

Communication

Motor stopped on command received from PLC or DCS.

Auto restart

Motor stopped by auto restart function.

Trip

Motor stopped due to trip.

No current

Motor stopped as the current is zero.

Forced Stop

Motor stopped on Forced Stop input.

Direction change

Motor stopped to change direction by reverse type of starters.

No feedback

Motor stopped as no feedback received (either current feedback or RUN DI).

Speed change

Motor stopped to change speed on command received (applicable for two speed starters).

Custom command

Motor stopped on Custom command detection.

Mode transfer

Motor stopped due to mode change if Bump mode is enabled.

No Voltage

Motor is stopped due to no voltage detected.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.