DOCA0257EN-01

Star Delta

Description

The Star Delta starter requires the following digital inputs and outputs:

  • Two inputs for motor local start and local stop.

  • Three outputs for motor RUN command, star connection (CONTACTOR OUTPUT 1), main connection (CONTACTOR OUTPUT 2), and delta connection (CONTACTOR OUTPUT 3).

Wiring Diagram

Example of wiring diagram of the TeSys Tera system in Star Delta mode:

KM1: CONTACTOR OUTPUT 1 (Star)

KM2: CONTACTOR OUTPUT 2 (Main or Line)

KM3: CONTACTOR OUTPUT 3 (Delta)

NOTE: Mechanical interlock is connected to KM1 and KM3.

Logical Diagram

The following diagram shows the logical diagram of the Star Delta starter:

Operating Principle

When Star Delta mode is selected, motor start is possible from one of the following sources:

If a start command is received from either of the above source and if the motor is ready to start (that is no inhibit cause detected) , then TeSys Tera system activates the star CONTACTOR OUTPUT 1 and main CONTACTOR OUTPUT 2 and starts the time in Star timer (T1 or delay 1).

Once the time in Star timer has elapsed, TeSys Tera system deactivates Star CONTACTOR OUTPUT 1 and starts the changeover timer (T2 or delay 2).

Once the changeover timer has elapsed, TeSys Tera system activates Delta CONTACTOR OUTPUT 3.

TeSys Tera system deactivates CONTACTOR OUTPUT 1, CONTACTOR OUTPUT 2, and CONTACTOR OUTPUT 3 if any of the following motor stop cause is detected:

DI/DO Default Assignment

When Star Delta starter type is selected, the default assignment and settings of digital inputs and digital outputs are as follows:

DI parameters

DI01 settings

DI02 settings

DI03 settings

DI04 settings

Trigger type

Active high

Active low

Active high

Active high

Input source

Local-START> DI

Local-STOP DI

Other

Mode Selection 1

Validation time

10 ms

10 ms

10 ms

10 ms

DO parameters

DO01 settings

DO02 settings

DO03 settings

Active type

Active high

Active high

Active high

Input source

CONTACTOR OUTPUT 1

CONTACTOR OUTPUT 2

CONTACTOR OUTPUT 3

Tag

CNTR OP 1

CNTR OP 2

CNTR OP 3

Output type

Level

Level

Level

Delay Settings

Parameter

Description

Setting range

Deafult value

Delay 1

Start timer

0.01 to 600.00 s in step of 0.01 s

10.00 s

Delay 2

Changeover timer

0.01 to 600.00 s in step of 0.01 s

0.30 s

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?