DOCA0257EN-01

Locked Rotor

Description

The Locked Rotor protection function protects the motor during the start of the motor. The Locked Rotor condition occurs mainly due to excessive load or due to improper connection between the rotor and the shaft. The Locked Rotor protection function is active only during the start time of the motor.

The Locked Rotor protection function generates the following signals:

  • Alarm: Any of the three-phase currents of the motor goes above the alarm level during the start of the motor.

  • Trip: Any of the three-phase currents of the motor goes above the trip level for the specified time delay during the start of the motor.

Parameter Setting

The locked rotor protection function has the following configurable settings:

Parameter

Setting range

Default value

Function

  • Disable

  • Alarm

  • Trip

  • Alarm + Trip

Trip

Trip Level

150–1000% of IFLC in step of 1%

200% of IFLC

Time Delay

0.1–6000.0 s in step of 0.1 s

10 s

Alarm Level

150–1000% of IFLC in step of 1%

200% of IFLC

Reset Mode

  • Reset key

  • DI

  • Communication

  • Auto

DI + Reset Key

Auto-Reset Delay (applicable only if Reset mode is Auto)

0.0–6000.0 s in step of 0.1 s

0 s

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?