DOCA0257EN-01

Name Plate

WARNING
UNINTENDED EQUIPMENT OPERATION
The application of this product requires expertise in the design and programming of control systems. Only personnel with such expertise should be allowed to program, install, configure, alter and apply this product. Follow all local and national safety codes and standards.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

The system settings can be set up using following interfaces:

  • A PC running the TeSys Tera DTM embedded in a FDT container such as SoMove software.

  • The LTMTCUF control operator unit

  • A PLC or DCS through the communication network.

Parameter name

Setting range

Default value

Tag*

MMR0000001

MMR0000001

Nominal Power

0.1–6553.5 KW

0.1 KW

Load Type

  • Motor

  • Heater

Motor

Number of Phases

  • Three Phase

  • Single Phase

Three Phase

Nominal Power

Nominal power value entered in name plate menu is reference for all power related protection.

NOTE: Full load current value is either IFLC based on the starter type selection and speed selected through motor commands.

Load Type

TeSys Tera system supports Motor (inductive) and Heater (resistive) as load types. You can configure the load type base on the load.

The default load type is Motor, that enables full functionality of TeSys Tera system based on the device configuration.

The following protection functions are disabled in Heater load type:

  • Thermal Overload

  • Locked Rotor

  • Stall Rotor

  • Maximum Number of Starts

  • Anti-Backspin Timer

  • Voltage Dip

  • Block Output

Direct Online starter can be used to control Heater Start or Stop in Heater load type.

Number of Phases

Select Three-Phase setting for three-phase motor, and Single-Phase setting for single phase motor.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.