DOCA0257EN-01

Temperature Measurement

The TeSys Tera system supports maximum 1 temperature inputs for LTMT main unit.

Temperature Measured by LTMT Main Unit

The LTMT main unit temperature input can be connected to a 2-wire temperature sensor.

One of the following types of temperature sensors can be used:

  • PT100

  • PTC (Binary)

Characteristic

PT100 temperature sensor

Binary PTC resistance temperature sensor

Range

25 to 100 °C

2700 to 4000 Ω

Resolution

0.1 °C

1 Ω

Refresh interval

500 ms

500 ms

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.