DOCA0257EN-01

HMI Communication Loss

Description

HMI Communication loss function:

  • Detects the loss of communication between the LTMT main unit and the HMI connected via the HMI port, once communication has been established.

  • Generates an alarm or a trip action according to the function setting.

Parameter Setting

Parameter

Range

Default value

Function

  • Disable

  • Alarm

  • Trip

  • Alarm + Trip

Disable

Time Delay

0.1 – 6000.0 s in step of 0.1 s

1 s

Reset Mode

  • Reset key

  • DI

  • Communication

  • Auto

DI + Reset Key

Auto Reset Delay

0.0 – 6000.0 s in step of 0.1 s

0 s

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.