DOCA0257EN-01

Frequency

Description

The LTMT main unit measures the frequency of the three-phase voltage supplied to the motor. The frequency function provides the value measured based on the phase 1 voltage. In case of loss of phase 1 voltage, the frequency is not measured.

Characteristics

Characteristic

Value

Unit

Hz

Resolution

0.01 Hz

Refresh Interval

20 ms

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?