DOCA0257EN-01

Current Imbalance

Description

The Current Imbalance protection function generates the following signals:

  • Alarm: Current Imbalance goes above the alarm level.

  • Trip: Current Imbalance goes above the trip level for the specified time delay.

NOTE: Current Imbalance protection function is not applicable in single-phase mode.

Parameter Setting

CAUTION
HAZARD OF MOTOR OVERHEATING
  • The Current Imbalance pickup setting must be properly set to protect the wiring and motor equipment from harm caused by motor overheating.
  • The setting you input must conform to national and local safety regulations and codes.
  • Refer to the motor manufacturer’s instructions before setting this parameter.
Failure to follow these instructions can result in injury or equipment damage.

The Current Imbalance protection function has the following configurable settings:

Parameter

Setting range

Default value

Function

  • Disable

  • Alarm
  • Trip
  • Alarm + Trip

Alarm + Trip

Trip Level

5–100% in step of 5%

20%

Time Delay

0.1–6000.0 s in step of 0.1 s

5 s

Alarm Level

5–100% in step of 5%

20%

Reset Mode

  • Reset key

  • DI

  • Communication

  • Auto

DI + Reset Key

Auto-Reset Delay (applicable only if Reset mode is Auto)

0.0–6000.0 s in step of 0.1 s

0 s

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?