DOCA0257EN-01

Communication Ports

The LTMT main unit has the following kinds of communication ports:

  • EtherNet/IP communication port

  • Modbus RTU communication port

  • PROFIBUS DP communication port

Ethernet Communication Port

NOTICE
unauthorized ethernet port usage
Use only one Ethernet communication port at a time, even though both ports are functionally identical.
Failure to follow these instructions can result in equipment damage.

The LTMT main unit with EtherNet/IP or Modbus TCP/IP communication protocols is equipped with two RJ45 Ethernet communication ports on the front face. They follow the Ethernet interoperability standards. It allows star and point-to-point connections. The main physical characteristics of Ethernet ports are:

Image

Connector

Description

RJ45 connector

  • Port 1

  • Port 2

Shielded ground terminal

For more information on wiring and connections, refer TeSys Tera Motor Management System EtherNet/IP Communication Guide - DOCA0258EN

Modbus RTU Communication Port

The LTMT main unit with Modbus RTU communication is connected to the Modbus field terminals by using a 4-terminal connector.

Image

Terminals

Description

D0

Data –

D1

Data +

Shielded earth

For more information on wiring and connections, refer to TeSys Tera Motor Management System Modbus RTU Communication Guide – DOCA0355EN.

PROFIBUS DP Communication Port

The LTMT main unit with PROFIBUS DP communication can be connected in the PROFIBUS DP daisy chain using two different connectors. In the LTMT main unit, standard DB9 connector is used for conventional method for PROFIBUS DP network. It can be achieved, by looping terminal available for PROFIBUS DP connection.

The maximum data speed with the different connectors are mentioned below.

Image

Connector

Data speed

D-type connector

12 Mbits/s

Terminal connector

1.5 Mbits/s

The PROFIBUS DP 4-terminal connector has the following pin assignments:

Terminal

Signal

Description
A RD-/TD- Negative data transmission (RD-/ RD-)
B RD+/TD+ Positive data transmission (RD+/ RD+)

Shielded earth
For more information on wiring and connections, refer to TeSys Tera Motor Management System PROFIBUS DP Communication Guide – DOCA0256EN.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.