DOCA0257EN-01

Motor Status

WARNING
UNINTENDED EQUIPMENT OPERATION
When the motor current drops below 10% of IFLC, the LTMCUF control operator unit displays 0. Make sure the motor is completely in the STOP position before carrying out any maintenance activities.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

The LTMT main unit defines the motor status based on maximum of three-phase current (IMAX) and full load current (IFLC) setting.

Motor status

Description

Stop

Motor stopped if IMAX < 10% of IFLC.

Start

Motor starting if IMAX ≥ 10% of IFLC.

Run

Motor running if IMAX goes above the Run threshold + 10% and comes below the Run threshold. Run threshold (RT) is a parameter of the Excessive start time function.

A Stop
B Start
C Run
D Stop

Heater Status

The LTMT main unit defines the heater status based on maximum of three-phase current (IMAX) and full load current (IFLC) setting.

Heater status

Description

OFF

Heater in OFF state if IMAX < 10% of IFLC.

ON

Heater in ON state if IMAX ≥ 15% of IFLC for 100 ms.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.