DOCA0257EN-01

LTMT Main Unit

The LTMT main unit is the main module of the TeSys Tera system which co-ordinates with different modules to provide features like protection, control, monitor, data storage, communication, and so on.

The LTMT main unit is available with following communication protocols:

  • Modbus RTU
  • PROFIBUS DP

  • EtherNet/IP and Modbus TCP/IP

The advantages of the LTMT main unit are:

  • The LTMT main unit provides power to the LTMTCT/LTMTCTV sensor module and LTMT expansion modules.

  • The LTMT main unit is independent of LTMTCT/LTMTCTV sensor module type. The LTMT main unit can be used for current-based protection or current and voltage-based protections.

  • The LTMT main unit can be mounted on top of the LTMTCT/LTMTCTV sensor module, which reduces width of basic module.

Except communication interface field bus, all the LTMT main unit connections remain same in all variants.

For more information on TeSys Tera system installation, refer to TeSys Tera Motor Management System Installation Guide – DOCA0356EN.

Front Face Description

A

Digital input connectors

B

RJ45 for LTMT expansion module connection

C

RJ45 for HMI and PC connection

D RJ45 ports for EtherNet/IP and Modbus TCP/IP communication
E

Device shield ground terminals

F

Temperature input connector

G

Power supply connector

H

QR code to product information page

I

Trip/Reset button

J

Status LED

K

Digital output connectors

Status LED

LED name

LED Color Indication

Description

Device

Off

Power Off

Green on

LTMT main unit is in healthy condition (turned on after power on self-test)

Green blinking

  • LTMT main unit is in logic test mode

  • Firmware upgrade check and firmware upgrade in progress

Red on

Internal error detected or configuration error detected

Red blinking

Communication between LTMT main unit and LTMTCT/LTMTCTV sensor module or LTMT expansion modules is lost.

Fallback (LTMTP•• and LTMTM••)

Motor

Off

Motor in Inhibit state

Green on

Motor in Stop state, ready to Start

Green blinking

Motor is running

Trip/Alarm

Off

No trip or alarm condition

Blue blinking

Alarm condition is present

Blue on

Pickup condition is present

Red blinking

LTMT main unit has tripped and trip condition is still present. Trip cannot be reset.

Red on

LTMT main unit has tripped and trip condition is not present. Trip can be reset.

NS*

Off

Not powered or no IP address

Steady green on

Configured client is connected and IO connection is established or device is in Fallback IP

Green flashing*

IP address is configured but no IO connections are established

Red flashing(6)

Communication loss or connection time out

Flashing green or red once*

During device power up self-test is performed

LK *

Off

No connection established 

Yellow steady

Link

Yellow blinking

Activity

ACT*

Off

10 Mbps speed 

Green steady

100 Mbps speed 

Comm*

Off

Communication is not established with PLC or DCS

Green on

Communication is established with PLC or DCS

Red blinking

Communication is lost with PLC or DCS

Trip/Reset Button

Use the Trip/Reset button to perform the following functions:

Function

Description

Procedure

Trip reset

Resets all trips that can be reset.

Press the button and release it within 3 s.

Self test

Performs a self test if:

  • No trips exist

  • Test mode function is enabled.

Press and hold the button for more than 3 s not exceeding 15 s.

Return to default values

Returns the LTMT main unit parameters to default values if the motor is in Stop state. If the motor is in Start or Run state, the return to default values is ignored.

Press and hold the button for more than 15 s not exceeding 20 s.

When the button is pressed for more than 15 s, the Trip/Alarm LED blinks in blue color.

The LTMT main unit parameters are reset to their default values when the button is released.

Induce a trip

Put the LTMT main unit into internal stucked reset key trip.

Press and hold the button for more than 20 s.

The LTMT main unit trips and trip is recorded in the Trips log.

Digital Inputs

The LTMT main unit has four potential free digital inputs (type 1 according to EN61131-2 standard).

The digital inputs can be powered internally through the LTMT main unit.

When the digital inputs are powered internally, the four digital inputs I.1, I.2, I.3, and I.4 can be used.

Digital Outputs

WARNING
UNIntended equipment operation
When motor is running with starter:
  • Under nominal condition: Digital output of LTMT main unit and LTMT expansion module will remain in NC state and follows the DO input source.
  • Under degraded condition: If LTMT main unit and LTMT expansion module cable is disconnected, the digital output of LTMT main unit will be in NO state, and the digital output of LTMT expansion module will continue in NC state.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

The LTMT main unit has three digital outputs:

  • Two outputs with NO contacts

  • One output with NO+NC contacts

LTMT Main Unit Temperature

A 2-wire PT100 or PTC temperature sensor can be connected to the LTMT main unit.

Expansion Port

The expansion port is used to connect optional LTMT expansion modules with the LTMT main unit. All LTMT expansion modules are connected in daisy chain.

LTMT HMI Port

The LTMT HMI port is used to connect the optional LTMTCUF control operator unit with the LTMT main unit. For more information on cables, refer Cables section.

The pinout of the shielded RJ45 connector of the LTMT HMI port is as follows:

Pin No.

Signal

Description

1

Not connected

2

Not connected

3

Not connected

4

D1 or D(B)

Transceiver terminal 1

5

D0 or D(A)

Transceiver terminal 0

6

Not connected

7

+5V

Auxiliary supply to LTMTCUF control operator unit

8

0VL

Signal and power supply common

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?