DOCA0257EN-01

RMS Current

Description

The LTMT main unit measures RMS values of line currents by using a LTMTCT/LTMTCTV sensor module.

  • IL1: Phase 1 RMS current

  • IL2: Phase 2 RMS current

  • IL3: Phase 3 RMS current

Characteristics

Characteristic

Value

Unit

Ampere (A)

Resolution

0.001 A

Refresh interval

20 ms

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?