DOCA0257EN-01

Calculated Ground Trip

Description

The ground current is an imbalanced current flowing through the neutral of the three-phase system. In normal conditions, the ground current is negligible or null. It is present only when a ground trip occurs.

DANGER
IMPROPER TRIP DETECTION
  • Calculated Ground Trip protection function will not protect people from harm caused by ground current.
  • Calculated Ground Trip pickup setting must be set to protect the motor and related equipment.
  • Calculated Ground Trip settings must conform to national and local safety regulations and codes.
Failure to follow these instructions will result in death or serious injury.

The ground current is calculated internally by the LTMTCT/LTMTCTV sensor module. The Calculated Ground Trip protection function generates the following signals:

  • Alarm: Calculated ground current goes above the alarm level.

  • Trip: Calculated ground current goes above the trip level for the specified time delay.

The protection function can be disabled when the motor is in Start state, to avoid nuisance tripping.

It is recommended to use the following for Calculated Ground Trip protection:

  • IFLCmin= 0.3 A in 0.3-3 A (similarly for 25 A and 100 A).

  • Minimum ground trip threshold = 50% of 0.3 A = 0.15 A.

NOTE:
  • If you keep protection setting below 50% of IFLCmin, then use measured ground trip with CBCT.

  • Calculated Ground Trip protection is not applicable in single-phase mode.

  • Hysteresis is not applicable for calculated ground current by setting less than 10% of FLC.

Parameter Setting

The Calculated Ground Trip protection function has the following configurable settings:

Parameter

Setting range

Default value

Function

  • Disable

  • Alarm

  • Trip

  • Alarm + Trip

Trip

Trip Level

10–500% of IFLC in step of 1%

20% of IFLC

Time Delay

0.05–600.00 s in step of 0.01 s

0.2 s

Alarm Level

10–500% of IFLC in step of 1%

20% of IFLC

Reset Mode

  • Reset key

  • DI

  • Communication

  • Auto

DI + Reset Key

Auto-Reset Delay (applicable only if Reset mode is Auto)

0–6000.0 s in step of 0.1 s

0.0 s

Function While Motor Starting

  • Disable

  • Enable

Disable

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.