DOCA0257EN-01

Load Current Transformers

External load current transformers expand the current range for use with motors greater than 100 A at full load.

Schneider Electric load current transformers

Primary

Secondary

Inside diameter

Reference

mm

In.

100

1

35

1.38

LT6CT1001

200

1

35

1.38

LT6CT2001

400

1

35

1.38

LT6CT4001

800

1

35

1.38

LT6CT8001

NOTE:
  • The LTMTCT3/LTMTCTV3 sensor module accepts 1 A and 5 A secondary signals from external current transformers.

  • The LTMTCT25/LTMTCTV25 sensor module accepts 5 A secondary signals from external current transformers.

  • 3 A and 25 A CT to be used for external CT.

For more information on external CT wiring, refer to TeSys Tera Motor Management System Installation Guide – DOCA0356EN.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.