DOCA0257EN-01

Under Power Factor

Description

The Under Power Factor protection function generates the following signals:

  • Alarm: Power factor (cos ɸ) goes below the alarm level.

  • Trip: Power factor (cos ɸ) goes below the trip level for the specified time delay.

NOTE: This function enables after 500 ms once the voltage is detected.

Parameter Setting

The Under Power Factor protection function has the following configurable settings:

Parameter

Setting range

Default value

Function

  • Disable

  • Alarm
  • Trip
  • Alarm + Trip

Disable

Trip Level

0.40–1.00 in step of 0.01

0.6 PF

Time Delay

0.1–6000.0 s in step of 0.1 s

0.1 s

Alarm Level

0.40–1.00 in step of 0.01

0.6 PF

Reset Mode

  • Reset key

  • DI

  • Communication

  • Auto

DI + Reset Key

Auto-Reset Delay (applicable only if Reset mode is Auto)

0.0–6000.0 s in step of 0.1 s

0 s

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.