DOCA0257EN-01

Device internal protection

Parameters Settings

The Device Internal protection function has the following configurable settings:

Parameter

Setting range

Default Value

Time Delay

0.1–6000.00 s in step of 0.01 s

1 s

Reset Mode

  • Reset key

  • DI

  • Communication

DI + Reset Key

NOTE: The Device Internal trip occurs if any of these diagnostic detected after the time delay. For more information, refer Device Internal Error Detected.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.