DOCA0257EN-01

Thermal Memory

Description

The LTMT main unit calculates the thermal memory based on the trip class and service factor parameters of thermal overload protection settings.

Characteristics

Characteristic

Value

Unit

%

Resolution

1 %

Refresh interval

20 ms

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.