DOCA0257EN-01

Reverse Direct Online

Description

The Reverse Direct Online starter requires the following digital inputs and outputs:

  • Three digital inputs for motor local start forward, local start reverse and local stop.

  • Two digital outputs for motor RUN forward command (CONTACTOR OUTPUT 1) and RUN reverse command (CONTACTOR OUTPUT 2).

Wiring Diagram

Example of wiring diagram of the TeSys Tera system in Reverse Direct Online mode:

KM1: CONTACTOR OUTPUT 1 (Forward)

KM2: CONTACTOR OUTPUT 2 (Reverse)

NOTE: Mechanical interlock is connected to KM1 and KM2.

Logical Diagram

The following diagram shows the logical diagram of Reverse Direct Online starter.

Operating Principle

When Reverse Direct Online mode is selected, motor start is possible from one of the following sources:

If a Forward Start command is received from either of the above source and if the motor is Ready to Start (that is no inhibit cause detected), then TeSys Tera system activates the forward main CONTACTOR OUTPUT 1.

Similarly, if a reverse start command is received from either of the above source and if the motor is ready to start (that is no inhibit cause detected), then TeSys Tera system activates the reverse main CONTACTOR OUTPUT 2.

The direction change logic depends on the Change Direction .

TeSys Tera system deactivates CONTACTOR OUTPUT 1, and CONTACTOR OUTPUT 2 if any of the following motor stop cause is detected:

DI/DO Default Assignment

When Reverse Direct Online starter type is selected, the default assignment and settings of digital inputs and digital outputs are as follows:

DI parameters

DI01 settings

DI02 settings

DI03 settings

DI04 settings

Trigger type

Active high

Active low

Active high

Active high

Input source

Local-START> DI

Local-STOP DI

Local-START< DI

Mode Selection 1

Validation time

10 ms

10 ms

10 ms

10 ms

DO parameters

DO01 settings

DO02 settings

DO03 settings

Active type

Active high

Active high

Active high

Input source

CONTACTOR OUTPUT 1

CONTACTOR OUTPUT 2

Trip

Tag

CNTR OP 1

CNTR OP 2

Trip DO

Output type

Level

Level

Level

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.