DOCA0257EN-01

LTMTCUF Control Operator Unit

The LTMTCUF control operator unit is a Human Machine Interface (HMI) that enables the configuration, monitoring, and control of the LTMT main unit, as part of the TeSys Tera Motor Management System

For information on installing the LTMTCUF control operator unit, refer to TeSys Tera Motor Management System Installation Guide – DOCA0356EN.

For information on using the LTMTCUF control operator unit, refer to TeSys Tera Motor Management System LTMTCUF Control Operator Unit User Guide – DOCA0233EN.

Front Face Description

The LTMTCUF control operator unit front face includes the following features:

A

LCD display

B

Contextual navigation keys

C

Front face RJ45 for PC connection (covered)

D

Local control interface, including five control keys and four LED

Rear Face Description

The LTMTCUF control operator unit rear face is shown in the following diagram:

A

Rear face RJ45

Status LED

In the diagram below, the four control LED are labeled A – D:

The following table describes each of the four LEDs:

LED

Status

Description

A

Motor ON/OFF status

CONTACTOR OUTPUT 1 is active

B

CONTACTOR OUTPUT 2 is active

C

Active mode status

The active control source is the Remote source

D

The active control source is the Local source (Local1, Local2, and Local3)

For more information, refer to TeSys Tera Motor Management System LTMTCUF Control Operator Unit User Guide – DOCA0233EN.

Control Keys

The local control interface consists of five control keys.

Key

Description

Run 1

Motor control keys

Run 2

Stop

Local/Remote

Active control source selection

Trip/Reset

Trip reset

For more information, refer to TeSys Tera Motor Management System LTMTCUF Control Operator Unit User Guide – DOCA0233EN.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.