DOCA0257EN-01

Current Phase Loss

Description

The Current Phase Loss protection function generates the following signals:

  • Alarm: Any of the three-phase currents of the motor goes below 10% of the motor full load current.

  • Trip: Any of the three-phase currents of the motor goes below 10% of the motor full load current for the specified time delay.

NOTE:
  1. Current Phase Loss protection function is not applicable in single-phase mode.

  2. Current values that are less than 10% of FLC are considered as stop, and no value is displayed in metering and trip logs.

Parameter Setting

The Current Phase Loss protection function has the following configurable settings:

Parameter

Setting range

Default value

Function

  • Disable

  • Alarm

  • Trip

  • Alarm + Trip

Trip

Time Delay

0.1–6000.0 s in step of 0.1 s

0.1 s

Reset Mode

  • Reset key

  • DI

  • Communication

  • Auto

DI + Reset Key

Auto-Reset Delay (applicable only if Reset mode is Auto)

0.0–6000.0 s in step of 0.1 s

0 s

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.