Circuits

The Circuits tab in Solution Center provides validation that you have all the Circuit Relationships in place. If necessary, expand each circuit to see the relationship properties.

IMPORTANT: To validate the relationships, your map service must be published and configured in Solution Center.

  1. In Solution Center > Fiber Manager > Feature Services > Fiber Manager, click Circuits.

  2. Under Relationships, expand each one. Green check marks indicate a successful validation.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.