Install Add-Ins for ArcGIS Pro

After the configurations are complete in Solution Center, you need to install the ArcFM Editor XI and Fiber Manager XI Add-ins.

To install the software:

  1. In Solution Center, click Rollout.

  2. In Rollout, click the Fiber Manager XI tab.

  3. Next to the Rollout version policy field, select the appropriate version of Fiber Manager XI.

  4. Click Copy Download Link.

  5. Paste the link in a browser to download the file.

  6. Back in Solution Center, click the Editor XI tab.

  7. Next to the Rollout version policy field, select the appropriate version of Editor XI.

  8. Click Copy Download Link.

  9. Paste the link in a browser to download the file.

  10. Close any open instances of ArcGIS Pro.

  11. Double-click the downloaded Editor XI Add-in.

  12. When prompted, click Install Add-in.

  13. Double-click the downloaded Fiber Manager XI Add-in.

  14. When prompted, click Install Add-in.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.