Configure the Structure Domain Network
A structure network is the hardware, such as ducts, conduits, and structure facilities, that supports all the communication lines. When you create a Utility Network (UN), a structure network is automatically created with predefined feature classes and tables.
To configure the Structure Domain:
-
From the home screen in Solution Center, click Editor > Editor Maps.
-
Select your operational map from the list.
-
Under Select a Domain Network to configure, select Structure.
-
On the Structure Setting tab, use these settings for the Fields:
Structure Setting
Field Name
Duct Diameter Units
Inches
Duct End Flag Annotation
DuctFlagEndAnno
Duct Flag Outline Annotations
DuctFlagOutlineAnno
MapUnits
Feet
MaxDucts
30
-
On the Structure Field Names tab, use these settings for the Fields:
Structure Field Name
Field Name
Description
Available
isavailable
Applies to DuctEnd features in the StructureJunction class, as well as to Duct objects in the StructureEdgeObject table, to indicate that the corresponding duct is eligible to receive a new occupant.
ConduitFacilityID
assetid
Identifier preferred by the customer implementing ArcFM, for conduit facilities.
DuctBankGuid
ductbankguid
Maintained by ArcFM Conduit Manager.
DuctDiameter
diameter
Floating point number that applies to Duct objects (StructureEdgeObject) and their corresponding DuctEnd features (StructureJunction). The length units associated with these values are specified by the DuctDiameterUnits configuration setting.
DuctEndGuid
ductendguid
Maintained by ArcFM Conduit Manager.
DuctEndShape
ductcrosssectionshape
Indicates the cross-sectional shape of the duct corresponding to a DuctEnd feature (StructureJunction).
DuctFlagLabelText
notes
Maintained by ArcFM Conduit Manager.
DuctFlagOutlineId
ductflagoutlineid
Maintained by ArcFM Conduit Manager.
DuctFlagRotation
ductflagrotation
Maintained by ArcFM Conduit Manager.
DuctFlagScale
ductflagscale
Maintained by ArcFM Conduit Manager.
DuctID
ductid
User-assignable identifier for a duct with a bank. Found on both the Duct (StructureEdgeObject) and its associated DuctEnd features (StructureJunction)
DuctOccupantDescription
occupantdescription
Maintained by ArcFM Conduit Manager.
LeaderLineAttachPoint
leaderlineattachmentpoint
Maintained by ArcFM Conduit Manager.
Material
material
NumberOfAvailableDucts
numavailableducts
Maintained by ArcFM Conduit Manager.
Occupied
isoccupied
(True/False) Indicates whether a duct is occupied. Automatically initialized by ArcFMConduit Manager while ducts are being edited, but user can assign an overriding value. Found on both the Duct (StructureEdgeObject) and its associated DuctEnd features (StructureJunction).
StructureAddress
name
Address of the structure.
StructureFacilityID
assetid
Structure identifier preferred by the customer implementing ArcFM.
WallHeight
wallheight
The height of the structure wall.
-
On the Send to Targets — Fields to Reset tab, Feature Class is the only section that needs to be configured.
-
Under Feature Class > StructureBoundary, click all options under Fields to Reset except Install Date, isavailable, and isoccupied.
-
Under Feature Class > StructureLine, click all options under Fields to Reset except Asset ID, depth, Design Type, diameter, Diameter Width, and distance.
-
Under Feature Class > StructureJunction, click all options under Fields to Reset.

-
-
Click Save.