Connections

In Fiber Manager XI, the Connections table keeps track of all fiber connections. Any time a fiber is connected to a port or a fiber is spliced to another fiber, an entry is made in the Connections table.

In Solution Center, you need to match the geodatabase data entries and attribute fields to this table. If you are using the Fiber Manager XI data model, the fields to map match the field names listed. If your database entry has different field names, make sure you connect the intended fields to the proper names.

The data from this table is used to populate Fiber Connections in ArcGIS Pro where you associate all your connections.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.