ArcGIS Pro Configuration for Fiber XI

The Utility Network (UN) provides the network topology rules that act as the foundation for the fiber optic system.

To build the UN, we provide a downloadable asset package to get you started out of the box. This asset package is a type of file geodatabase that models the schema, properties, related layers, related tables, and data of a UN. It contains the definitions and parameters of the Fiber Manager XI Data Model that enables a transition between databases for data design, loading, and rollout.

This data model contains sample data and aligns with UN requirements as follows:

  • Feature layers are modeled based on UN asset groups and asset types.

  • Assets contained in the equipment hierarchies that are children of feature layers are modeled in related tables.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.