Schematic Display Fields

The Schematics tab is where you can configure up to seven display fields for the cables and splices in the Fiber Splices schematic.

To add a new field to the schematic, follow these steps:

IMPORTANT: The order in which you add the fields is the order in which they are displayed. We recommend that you plan out which fields you want and in what order first, then follow that order when adding the fields.
  1. For either the Fiber Cables or Splice Points, click Add New.

  2. Use the drop-down to choose the appropriate field.

  3. Click Apply.

  4. If necessary, click the Edit change the field.

  5. If necessary, click the Remove to eliminate the field.

  6. Click Save.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.