Reports

The reports tab lets you configure specific cable, splice, trace, and circuit stylesheet parameters for individualized reports.

To set up your report format:

  1. Log in to Solution Center and click on the Fiber Manager plugin.

  2. On the Feature Services tab, select the applicable map from the list.

  3. On the left side menu, click the Reports tab.

  4. Select Splice Report XSL from the Report Style Sheets menu. Next to Splice Report Format, click CSV and click Save. Next to Splice Report Format, click HTML and click Save again.

    This saves the default style sheets format for each report type.

  5. Repeat Step 4 for the Trace, Cable, and Circuit Trace report formats.

  6. To put the changes into effect in the feature service, you must restart your map service in ArcGIS Server.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?