Create Circuit Relationship

A connectable object is any fiber asset that can be viewed or edited in the Fiber Connections pane. All connectable objects require a relationship with the Circuit table, so if you create a new connectable object, you must create the Circuit relationship too.

The Circuit table is always the Origin (parent). The connectable objects and the Connections table are the Destination (child).

If you are using the ArcFM Fiber Manager XI Data Model and Sample Data, these objects already have a circuit relationship:

  • ActiveCommonPort

  • ActiveSplitPort

  • BackPort

  • Connection

  • DevPort

  • FrontPort

  • PassiveDeviceCommonPort

  • PassiveDeviceSplitPort

  • RibbonStrand

  • SplitIn

  • SplitOut

  • Strand


To create a relationship:

  1. Open the Create Relationship Class geoprocessing tool.

  2. Follow the table and enter the parameters.

    All circuit relationships follow the same configuration pattern:

    Create Relationship Class Parameters

    Value

    Origin Table

    Circuit

    Destination Table

    The Connectable Object Table, for example, Strand

    Output Relationship Class

    This is where the relationship is saved, but it is also an opportunity to name the relationship.

    Relationship Type

    Simple

    Forward Path Label

    This label is not used by Fiber Manager XI. It is seen within ArcGIS Pro’s Attribute tables. For Forward Path, you can choose the name of the destination (or child) table.

    Backward Path Label

    This label is not used by Fiber Manager XI. It is seen within ArcGIS Pro’s Attribute tables. For Backward Path, you can choose the name of the origin (or parent) table.

    Message Direction

    None (no messages propagated)

    Cardinality

    Many to many (M:N)

    Attributed

    Check the box for “Relationship class is attributed.” After the relationship is created, you add attribute fields to the table.

    Origin Primary Key

    globalid

    Origin Foreign Key

    orig_fky

    Destination Primary Key

    globalid

    Destination Foreign Key

    dest_fky

  3. When complete, click Run. Repeat step 2 for each new object created.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?