Export the Asset Package

When your testing and review of the asset package is complete, you can create your own asset package. This new package represents your updated data model you can use with an enterprise geodatabase, store as a backup, and deploy on other ArcGIS Pro instances and tenants. See Apply the Asset Package for more information.


To export your files:

  1. Open the geoprocessing pane and search for Export Asset Package.
  2. In the window that opens, drag the Utility Network (UN) to the Input Utility Network field.

  3. Enable the Domain Networks and Include data boxes.

  4. Review the export Folder Location and click Run. Save the exported file for future use.

    NOTE: This tool can take 10–15 minutes to run.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.