Configure the Fiber Manager SOE

Server object extensions(SOEs) allow you to create new service operations to extend the capabilities of your GIS server. After the SOE is installed, you configure it as a Capability on the Fiber Manager XI map service.

NOTE: If any SOE parameters are changed, you must restart the feature service for the changes to take effect.

To configure the SOE:

  1. At the top of ArcGIS Server Manager, click Services. The Manage Services tab is selected.

  2. Scroll down to your listed map service and click the name. The Edit window opens.

  3. On the left-hand side, click Capabilities.

  4. Under the Select and Configure Capabilities heading, check the box next to FiberXIRestSOE. Then, click the text.

  5. Scroll down to the Properties heading. Use the table as a guide to populate the values. You can get the layers’ and tables’ ID numbers from the published feature service URL.

    Property

    Value

    OrganizationName

    The tenant name.

    CommJunctionLayerIndex

    This is the ID of the Communication Junction layer as found in the published map service.

    MapName

    This is the Map Name as found within the published map service.

    ServiceBusTransportType

    Enter one of the two possible values.

    • AmqpTcp - The connection uses the AMQP protocol over TCP. This is the default protocol used when no value is provided.

    • AmqpWebSockets - The connection uses the AMQP protocol over web sockets. This would be used if the connection must go through a proxy.

    CommLineLayerIndex

    This is the ID of the Communications Line layer as found in the published map service.

    DiagnosticLogToFile

    This setting logs additional error information related to the Fiber Manager XI SOE that could be beneficial for Schneider Electric troubleshooting.

    Leave the setting at the default value of “0.” Only change this setting if directed by the Schneider Electric Support Team. If needed, the file is saved in the local ArcGIS Server user account directory. This is one example: C:\Users\siteadmin\AppData\Local\ESRI\Server10.9\EntAssemblyCache\{BA2DD96E-2245-481E-84DA-31A24A52C14D}\FiberXIRestSOE_DiagnosticFile.txt

    DomainNetworkName

    This is the string before the UN layers as found in the published map service. Example: Communications Junction (2). Communications is the name.

    ClientSecret

    This ClientSecret is generated as a part of creating an API key for the SOE. This API key must have the Editor.Admin and Fiber.Admin role.

    ClientID

    This ClientID is generated as a part of creating an API key for the SOE. This API Key must have the Editor.Admin and Fiber.Admin role.

    FiberFeatureServiceID

    This is the unique map ID for the published map service as found in Solution Center > Editor > Editor Maps.

    TenancyServiceURL

    This is the URL that tells the SOE which tenant to use. Type the following URL:

    https://tenancy.arcfmsolution.com

  6. When complete, at the top of the window, click Save and Restart.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.