Open the ArcGIS Pro Project File

After the add-ins are installed in ArcGIS Pro, download the ArcGIS Pro editing project for Data Model. This pre-configured project file has basic symbology, label expressions, and predefined mapping capabilities that let you start working with ArcGIS Pro right away. When you import the favorites file, you can start editing your map with pre-configured Fiber Manager objects.

The first time you open ArcGIS Pro with the Add-ins installed, you are prompted to log in to your tenant. This is the same tenant you log in to with Solution Center.

If you are using the Fiber Manager XI project file, you will need to connect the project to your published data source.

  1. Open the project file and log in to both your ArcFM account and Portal for ArcGIS account. Because the ArcGIS Server is connected to the portal, your database assets are listed in the Contents pane.

    It is normal to see a notification from ArcGIS Pro that it cannot find the operational map.

  2. In the Contents pane, click one of red exclamation points to repair the data source.

  3. In the Change Data Source window that opens, click ArcGIS Enterprise from the left hand menu.

  4. Click the name of your published feature service and click Open.

  5. Now click the table name that matches the asset you clicked on, then click OK. In this example, Communications Junction Object matches the one from the Content pane and click OK.

Before starting any editing tasks, we recommend you check the feature layer names between the editing package, the configuration in SC, and the published feature service.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.