About Signal Strength
Signal Strength Indicator
There is four different levels of signal strength:
Good Signal (between 0 & -54dBm)
Normal Signal (between -54 & -79dBm)
Poor Signal (<-79dBm)
No Signal (device is offline)
Cause of Poor Signal
Connectivity issues can be caused by various factors, such as:
-
Distance between the Wiser Hub and devices: The signal becomes weaker as the devices move farther apart.
-
Physical Obstructions: The doors, walls, furniture, household appliances, especially with metal surfaces, and other electronic devices can weaken the Zigbee signal.
Troubleshooting
-
Place the Wiser Hub into open space.
-
Make sure you check if all powered devices are switched on and working normally.
-
If possible, move the Wiser Hub closer to the device with signal issues.
-
Try to remove any physical obstructions between the Wiser Hub and the device with poor or no signal.
Help & Support
If you require further assistance, visit our Wiser Support Pages.