SUG_Wiser-00

Operating Elements

A

Ethernet port

This port is used for connecting the Ethernet cable to establish a wired network connection.

B

Power adapter port

This port is used for connecting the power adapter cable to supply power to the device.

C

LED Indicator

Displays the status of the Wiser Hub.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?