SUG_Wiser-00

List of Devices

On the Devices screen, you can find all installed devices of your Home, sorted by their device type. The devices will also display their Name and Room location.
  1. On the Home screen, tap Devices > Devices.

You can see the list of Devices:

A

Tap + to add new devices to your home.

B

Tap and enter the device name in the search bar to find it.

C

Tap refresh button to update the device list.

D

Tap the power button to turn the device ON/OFF.

E

Tap to remove the device from the Wiser System.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?