SUG_Wiser-00

Automate

Automate allows you to set a timer to automatically turning OFF devices after a specified period. For example, if you set a Auto-OFF timer for 30 minutes to turn OFF the light, the light will automatically turn OFF after 30 minutes of being turned ON.

Auto-OFF Timer

  1. On the Home screen, tap Devices > Devices.

  2. Select Wi-Fi® devices for which you want to set Auto-OFF Timer.

  3. On the Device Control screen, tap Schedule.

  4. Tap the toggle button to enable Auto-OFF Timer.

  5. Tap to enter the time.

    NOTE: You can not enter the time without enabling the toggle button.

Presence simulation

Presence simulation allows you to set connected loads to turn ON or OFF for random intervals of time.

For example, you can set the living room light to turn ON or OFF at random times in the evening. This makes it look like someone is at home, even when you are away.

Tap the toggle button to enable or disable.

NOTE: This feature is only recommended for lighting loads.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?