SUG_Wiser-00

Creating a Schedule

You can create a schedule using the Wiser app.
  1. On the Home screen, tap Devices > Devices.
  2. Select Wi-Fi® devices for which you want to create a schedule.
  3. On the Device Control Screen, tap Schedule.
    The Schedule screen appears.
  4. Tap Schedule > +.
  5. Tap (A) and enter the name of the schedule.
  6. Select the ON time and OFF time (B) as per your preference.
  7. Select the fan speed (C).
    TIP: The controlling options can vary based on the type of device you select. For example:
    • Fan Controller: Set the fan speed.

    • Dimmer: Adjust the brightness percentage.

    • Curtain Controller: Set the percentage of shutter opening.

  8. In the Perform on section (D), select one of the following options:
    • Weekdays: The schedule will apply to all weekdays.

    • Weekend: The schedule will apply only to weekends.

    • Only once: The schedule will apply to that particular day.

    You can also select random days without choosing these options, so the schedule will apply to those specific days.

  9. Tap Save (E).
The schedule will be successfully created and added to the Schedule tab. Tap the toggle button to turn the schedule ON or OFF.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?